Tool/software: Code Composer Studio
hi i tried to transmit
I2cWrite("1234567891234567891234567891"); //see the red marked "1", now it is not working if above 27 character is transmitted
hi tried to write the above string but it fails to write on I2C channel,
I2cWrite("123456789123456789123456789");//see the red marked "1" is removed here, now it works fine, if the total string is 27 or less,
how to increase the total number of string to transmit.
thanks