Tool/software: Code Composer Studio
At the time of returning from function facing a problem of no source available in CCS 5.5.0,please help me solving this issue
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
At the time of returning from function facing a problem of no source available in CCS 5.5.0,please help me solving this issue
Hello Shreya,
The "error" is not really an error. It is a message from the debugger telling you that the target is halted at a program address where there is no source association. Whether that address is a valid address or not depends on the program. If you are expecting to get to main, have a breakpoint set there, and never reach it, it could be that there is some issue with either your target or you program (or maybe both).
Can you try run a example project with the same target and see if you still have the same issue?
Thanks,
Yiding
Thanks Yiding ,
As you said that target is halted at program address i know that and address 0x37ce contain 0000 ,if i put break point from where it happens then it jump to the next memory location ,is it the problem of memory or ccs or any other things.
Thanks team,
Issue is in buffer which i have written i'm taking size of an 20 buffer and at the time of clearing clearing 40 that's why i thing issue is occurring and also after executing one more command that issue was coming i'm working on that.
**Attention** This is a public forum