Hello,
In reading the datasheet the memory address for the beginning of code (program) space is 0x8000 to 0xFFFF. When I look at my assembly in code composer it actually starts at 0x882A as shown in the attached screenshot. I'm thinking this is define by the linker?
The reason I'm looking into this is because I need to send the MSP an updated image/bit file via the BSL and I need to figure out where exactly to put it.
Questions
1. Can I just use the address shown in the debugger - 0x882A and the MSP will be happy?
2. Why is the program code not at 0x8000?