Other Parts Discussed in Thread: CC3100, CC31XXEMUBOOST, CC3200, CC3135, CC3120
Hello,
I need to buy MCU for my project which the goal is an IoT device which can act as an HTTP client. I need to confirm the compatibility and choose which MSP MCU to choose. Below is my concern:
1. I can see that MSP430F5529 need CC3100 to connect to WiFi. What about MSP432P401r, does it need CC3100 as well or it needs another variant?
2. If I am going to use MSP430 with CC3100 and Kentec boosterpack together, are they compatible to stack those boosterpack together? I can see that both boosterpack using SPI. Can they work at the same time? I understand that we can have multiple slaves in SPI. Do I need to configure something (eg: slave address or something else) to make it work together.
3. If I need CC3100, do I need to buy the CC31XXEMUBOOST as well?
I hope the question asked is clear. I don't want to repeat the same mistake before which I bought Kentec boosterpack to be used with CC3200 which is not directly compatible and I had painful process integrating it together. Now I need to buy new MCU since my CC3200 is fried unexpectedly while programming it. So, I decided to change into MSP MCU since it has vast community and a lot of resources online. Thank you in advance.
Best regards
Khairul