Other Parts Discussed in Thread: MSP-EM-DESIGN-CENTER, TIDM-1PHMTR-ESD
Dear Sir/madam,
I want to connect the GUI of the EVM430-F6736. So as described in "SLAA517E-May 2012 REvised August 2015" on page 20 and 21, I have decompressed the zip folder and started the application. Instead of the window on page 21 with the program, only a console opos up and closes again immeditely. No error message, nothing ! It is frustrating.
Why doesn't the file calibrator.exe work? I use Windows
I have looked that there is a serial connection:
The COM7 is connected to the current meter.
Furthermore, the files are all decompressed:
When I run "calibrator.exe", then just a black window pops up for milliseconds and closes immediately. When I run this from the console, then also another black window pops up. No error message is visible, nothing. What am I doing wrong?
Help is very much appreciated. Many thanks in advance.
Best regards
Patrick