Part Number: BOOSTXL-SENSORS
Hi,
I need some guidance on the launchpad and accessories, I want to attach multiple boost-xl modules to receive several analog signals. I would like to collect analog signals from 6-8 sensors, and then the launchpad would do some computations on the 6-8 signals to output 6 signals. The 6-8 signals are load cell signals that require computations/processing using either a 6x6 matrix or a 6x8 matrix to give 3 force outputs and 3 moment outputs for a total of 6 outputs. See example below where the D1-D6 are the analog signals and the R1-R6 are the computed outputs.
Is this possible with the boostxl launchpad? Is there any training/videos to help with this?
Thanks,
Adamlaunchpad matrix.docx