Part Number: MSP-FET430UIF
Hello.
I have an MSP-FET430UIF pod with V1.4a hardware. The pod has been "bricked" or messed up during a previous firmware upgrade from within a development tool (don't remember which tool).
The point is that the pod is now dead. I assume I could simply reprogram the MSP430F1612 microcontroller in the dead pod if I have another working pod (which I do). I would simply reprogram the processor on the dead pod board just as if it were any other MSP430 target board we would develop in-house. The only problem is I need the firmware HEX file for the FET430UIF pod.
I have another working FET430 programmer, and I know how to wire between the working pod and the 7-PIN header on the dead pod board. I just need the appropriate firmware file (HEX file) for the V1.4a pod. I would prefer firmware version 3.04.01.000 as this mates nicely with my PC application programming tool (I now use Elprotronics FETPro 430), but I will take any version 3.xx that is available.
Please can someone at TI or other E2E member point me to this HEX file.
Thank you.