I am using the MSP430F47166 with LCD_A module driving a 4-mux LCD and would like to control the contrast via software with the VLCDx bits. The project was initially designed with a resistor ladder of 680 kOhm resistors, with a 0 ohm from R03 to ground. The user's guide mentions the necessity of a 4.7uF cap or larger on LCDCAP/R33 if the internal charge pump is used. Should I have the resistor ladder AND the 4.7uF cap, or are these components mutually exclusive?