Other Parts Discussed in Thread: MSPWARE
Hi experts,
Please tell us about "Table 5-29. 12-Bit ADC, External Reference" in the datasheet.
Q1: When using VeREF+, is it OK to supply a voltage below 1.2V? (Specifically, 0V is supplied.)
We would like to use an external power supply for the ADC reference voltage.
While the ADC is in use, it provides 3.3V to the VeREF+.
However, I would like to stop supplying 3.3V and supply 0V while not using the ADC.
The content of "Table 5-29. 12-Bit ADC, External Reference" does not mean that a voltage below 1.2 should not be added, but can be interpreted as requiring at least 1.2V when using the ADC.
MSP430FR599x, MSP430FR596x Mixed-Signal Microcontrollers datasheet
Q2:Is it necessary to set the GPIO pin before supplying 0V as a workaround when 0V cannot be used for VeREF+?
Or, if you have any other workarounds, please let me know.
Best Regards,
O.H