Part Number: MSP-EXP432P401R
Tool/software: TI C/C++ Compiler
I tried troubleshooting software/ hardware issues and realized that it could be something wrong with my com ports. I purchased an HP laptop thinking I needed Windows and spent all day today downloading and reinstalling everything. I am still getting the same error.
I have installed all tools and downloaded the MSP432P4 drivers. Still did not help. This is for a class. I am running behind. I'd appreciate resolving this issue asap.
Thank you
This is the error I am receiving:
Energia: 1.8.11E23 (Mac OS X), Board: "RED LaunchPad w/ msp432p401r EMT (48MHz)"
Sketch uses 35024 bytes (13%) of program storage space. Maximum is 262144 bytes.
Global variables use 6500 bytes (9%) of dynamic memory, leaving 59036 bytes for local variables. Maximum is 65536 bytes.
DSLite version 9.2.0.1793
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: CS_DAP_0
Executing Startup Scripts: CS_DAP_0
Initializing: CORTEX_M4_0
Executing Startup Scripts: CORTEX_M4_0
Connecting...
fatal: CS_DAP_0: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 8.3.0.00003)
Failed: Operation was aborted
the selected serial port Failed: Operation was aborted
does not exist or your board is not connected
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.