Hi everyone,
I am trying to use BSL to download our upgrade firmware into MSP430f168 via serial port.
As the device is packed the only way that I have access to MCU is UART1 which is set 19200m, No Parity, 8bits, 1 stop bit.
I am using CCSv4 as compiler can set the output to get .txt file however I am not sure it's the file I need.
I have tried to rest the device and send following BSL command after reset assuming the default setting after reset is 9600, even, 1stop
TO BSL: 80
(Synchronization character sent to the BSL)
FROM BSL: 90 (Acknowledge from BSL)
TO BSL: 80 14 04 04 F0 0F 0E 00 85 E0 (Send Command to read memory from 0x0F00, length 0x000E)
FROM BSL: 80 00 0E 0E F2 13 40 40 00 00 00 00 00 00 02 01 01 01 C0 A2
(Returned values from BSL)
so far no any success , any help and experience is appreciated.
Thanks,