Hi,
I cant seem to find in the user guide how to set up the VBAT pin on the MSP to be a battery backup for the RTC. I want to be able to use the VBAT to power the RTC if/when the main power is lost.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I cant seem to find in the user guide how to set up the VBAT pin on the MSP to be a battery backup for the RTC. I want to be able to use the VBAT to power the RTC if/when the main power is lost.
Hello,
This is the function of Hibernation module.
The Hibernation module power source is supplied by VDD as long as it is within a valid range, even if VBAT > VDD. The Hibernation module also has an independent clock source to maintain a real-time clock (RTC) when the system clock is powered down. Hibernate mode can be entered through one of two ways: • The user initiates hibernation by setting the HIBREQ bit in the Hibernation Control (HIBCTL) register • Power is arbitrarily removed from VDDwhile a valid VBAT is applied.
Please see the Hibernation module in Technical Reference Manual for detailed configuration. An example is as below:
**Attention** This is a public forum