Other Parts Discussed in Thread: ENERGYTRACE, , MSP-TS432PZ100
Tool/software: Code Composer Studio
In order to be able to use the EnergyTrace+ functionality I just purchased an MSP-FET Flash emulator (Rev 2.0.6) to debug an MSP-EXP432P401R LaunchPad (Rev 2.1) by using an MSP-FET-432ADPTR (Rev 1.0), however it does not seem to work. I have selected "TI MSP430 USB1" for 'Connection' in the project settings, but I always get the following error message in CCS V. 10.1.0.00010 :
"CORTEX_M4_0: Error connecting to the target: Unknown device"
I am using the 10-pin ribbon cable to connect the MSP-FET432ADPTR to the LP MSP432 In connector. The FET432ADPTR switch S1 is in the position "Vcc Sense" (External Power) as I provide the power for the MCU with the LP usb cable. I removed all the LP J101 jumpers apart from the GND, 5V and 3.3V ones.
I also tried the "MSP-FET HID Cold Boot" procedure described on paragraph 5.6.5.3 at page 20 of SLAU647H. Launching the debug session I have been presented with the expected Recovery confirmation dialog, followed by automatic firmware update window. see pictures below
then the update...
but at this point I still obtain the "unknown device" error:
Installation details:
I have the same error by using the same hardware setup in CCS 9.3
Could you please help me to resolvine this issue ?
Francesco