Hello All,
I'm having difficulty with the following lines, which are contained with SlNetIf.c and therein the SlNetIf_add(..) function
I suspect the issue is with the ifConf argument (the right-most argument) passed into the function call. As seen in the following screenshot.
I use SlNetIf_listHead, which at the time of calling set to NULL. However, this is the only argument of type SlNetIf_Config_t that I have found which gets me to this point without an ISR fault or returning an error code.
Here is the code that preceeds ifCreateContext call, in case it helps.
I have failed to locate the definition and declaration of the ifCreateContext call. This may also be the issue. When stepping through using the debugger, the program jumps to an ISR fault infinite while loop the instant that line 1091 (screenshot 2) runs.
Thank you in advance for your help
EDIT:
When using the "step into assembly" option at that line (line 1091), I get the following message.
I don't know if that helps at all, but I thought I should append it to my post.