If TIDM-TWOPHASEMETER-I2040 design doesn't use Neutral and use only two phase then , can i use this design ? Because I want to use for phase to phase , 440V heater supply monitoring.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If TIDM-TWOPHASEMETER-I2040 design doesn't use Neutral and use only two phase then , can i use this design ? Because I want to use for phase to phase , 440V heater supply monitoring.
Hello Gaurang,
Yes that should work. You need to use one “phase” or connection as the reference or GND. You also need to adjust the voltage resistor divider to ensure the higher voltage doesn’t damage the ADC.
**Attention** This is a public forum