This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

MSP430BT5190: Is it possible to update FW through OAD using CC2650

Prodigy 180 points

Replies: 1

Views: 27

Part Number: MSP430BT5190

Hello,

We're using the MSP430BT5190 with the CC2650 in our design, and we were wondering the following. If we implement OAD to upgrade the CC2650 firmware, would it also be possible to upgrade the MSP430BT5190 firmware through the CC2650 OAD? From this link, It looks like this would be possible with the MSP432 family, just wanted to see if something similar were possible with the MSP430BT5190.

If not, is there another way that we could implement this? For example, could we use the CC2650 to download/store the firmware update for the MSP430BT5190, and then use the CC2650 to program the bootloader.

Thank you for the help here!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.