This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5338: upgrading from msp430ware_0_00_00_10

Part Number: MSP430F5338
Other Parts Discussed in Thread: MSP430WARE, MSPWARE

Tool/software: Code Composer Studio

Champs,

customer needs to upgrade a project that was originally developed long time ago using CCS4 and msp430ware_0_00_00_10. as a side note: the PC that was used to run the build has died

The project imports into CCS10 with no problem and after installing ti-cgt-msp430_4.4.8 compiler I am able to invoke build which in turn (obviously) fails. I tried using latest mspware but encountered multiple errors due to differences in folder structure as well as file names and functions. To my understanding the options are:

1. get msp430ware_0_00_00_10 and build the project against this version

2. port the project into latest mspware which would incur non-negligible development effort

options 2 seems to be the last resort here since it is not a new development, they just need an occasional tweak/build.

Would it be possible to make msp430ware_0_00_00_10 available for the customer?

thank you

Michael

**Attention** This is a public forum