Other Parts Discussed in Thread: SYSCONFIG
Hi,
I have interfaced MSP430i2040 and CC1352 via UART and reused the Design Center code[of MSP430] in my CC1352 to receive electrical parameters. Though I am able to get VRMS, IRMS, VPeak, IPeak and Power Factor, but unable to receive active_power, frequency, reactive power, Apparent Power etc parameters. As soon my device is powered MSP430 continously sends data and my callback is called and data is received.
If I connect the TX and RX of MSP430 of my board to the MSP430 Evaluation board, then I get all correct parameters which I can see in the GUI based pc application provided by TI.
These are my CommandHandler_registerCmdListeners() :
Comm_addCmdListener(COMMAND_HANDLER_EM_GUI_ID_BYTE,
COMMAND_HANDLER_VRMS_ID,
&Handler_vrms);
Comm_addCmdListener(COMMAND_HANDLER_EM_GUI_ID_BYTE,
COMMAND_HANDLER_IRMS_ID,
&Handler_irms);
Comm_addCmdListener(COMMAND_HANDLER_EM_GUI_ID_BYTE,
COMMAND_HANDLER_VPEAK_ID,
&Handler_vpeak);
Comm_addCmdListener(COMMAND_HANDLER_EM_GUI_ID_BYTE,
COMMAND_HANDLER_IPEAK_ID,
&Handler_ipeak);
Comm_addCmdListener(COMMAND_HANDLER_EM_GUI_ID_BYTE,
COMMAND_HANDLER_POWER_FACTOR_ID,
&Handler_power_factor);
Comm_addCmdListener(COMMAND_HANDLER_EM_GUI_ID_BYTE,
COMMAND_HANDLER_FREQUENCY_ID,
&Handler_frequency);
Comm_addCmdListener(COMMAND_HANDLER_EM_GUI_ID_BYTE,
COMMAND_HANDLER_ACTIVE_POWER_ID,
&Handler_active_power);
Comm_addCmdListener(COMMAND_HANDLER_EM_GUI_ID_BYTE,
COMMAND_HANDLER_REACTIVE_POWER_ID,
&Handler_reactive_power);
Please suggest me how can I debug the issue. ?
Regards,
Praveen T V