Other Parts Discussed in Thread: DRV8343S-Q1EVM,
Hi,
Tommy directed me to this forum regarding a question on RC values for MSP430F5529 MCU low-pass filtering used in DRV8343S-Q1EVM board. The current sensing pins, ISEN_A, ISEN_B, ISEN_C use R=56 ohms and C=2200pF, which leads to very fast time constant, about 120 ns. I check the datasheet of MSP430F5529, minimum sampling time is 1000 ns in Section 5.36 in page 42 of the datasheet. Assuming 1% error, 5 times RC equals to 600 ns, which is smaller than the minimum sampling time of 1000 ns. I am wondering whether the RC values are correct in this EVM board design. Please advise.
Another question is which frequency the TIDA-DRV8343S-Q1EVM design try to filter? For 45KHz PWM, it seems to me that above 45KHz frequency should be filtered. If this is the case, RC should be about 1/(5*f_sw) = 4.5 us. From this perspective, both R and C should be larger. My understanding is that C value should be larger than C_SAMPLE inside the MCU so that C_SAMPLE can be fully charged. Does the MCU has a maximum RC value limit? If yes, what is it?
I will appreciate your insight in RC filter design for ADC.
Thanks,
John