Dears
I want to configure BOOTCFG Register in order to use Rom Bootloader,
please give any sample code in c for do that, While reading Data sheet
I feel confused ,Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears
I want to configure BOOTCFG Register in order to use Rom Bootloader,
please give any sample code in c for do that, While reading Data sheet
I feel confused ,Thanks
Hello Rajeshkumar,
You can find some examples in the Simplelink MSP432E4 SDK, like boot_serial_i2c_flash, boot_serial_uart_flash. They have examples of setting the configuration.
Srinivas
Dear Srinivas
1, This Examples is for Flash based Boot loader , I want to use USB DFU Present in ROM Boot loader ,
2. In data sheet it is mentioned as to config Boot config Register using FMD , but I feel confused
3. for how to commit or Config Bootconfig Register , using FMD Register ,FMC Register
4. my Requirement is to Config, Bootconfig Register to use USB DFU ROM bootloader
so only I asked example code for that ,but the example i link you recommended is for flash based boot loader
Dear Srinivas
Today I ,have Successfully Activated USB ROM Bootloader and Flashed bin file using LM flash programmer
in msp432e401y launchpad Development Board
Thanks for your support.
**Attention** This is a public forum