Other Parts Discussed in Thread: MSP430F5528, , TXB0104, TXS0102, MSP-ISO
I’m using a MSP430F5529LP as a status monitor for my other electronics. I have built a board to interface my electronics to the launch pad much like a boosterpack board. This board is powered and provides 3.3 volts to the MSP430 with the 3.3V jumper removed on the launch pad. This is done because I will not normally connect the launch pad to a USB port. The MSP430 does not run because it seems the SBW-RST jumper must be removed. If I do that my code on the MSP430 starts and runs fine. Only issue is that I want to retain the ability to connect the USB and update my code running on the MSP430 which does not seem possible if the SBW-RST connection is missing. Do I need to connect a FET where the SBW-RST jumper goes and have it switch on when the USB cable gets connected or am I missing something.
Thanks for you help.
Some general information about what I’m using on the MSP430
I2C to talk to an LCD display and read temps sensors, ADC channels to read system power supply voltages and GIPO to read status bits from other boards and control power up down sequencing.