Other Parts Discussed in Thread: CC1101,
Hi there,
I'm using timer A to wake up MCU from LPM3 and do spi cumnication with CC1101 radio. Although I configured spi pins as input after the comunication is done , notice that SIMO stays high. I used module A1.
When I switch to spi module B0 I have no issue.
My question is what is cuasing SIMO in module A1 to stay high even when there is no data to comunicat and it configured as input afer the comunication is done ?
I sourced my timer A from ACLK which using the VLO.
SPI clock is 1 MHz and sourced from SMCLk.
I'm using custom board based on msp430fr5989 rev C.