Part Number: MSP432P4111
I have a custom board and am using the MSP-EXP432P4111 Launchpad board's XDS110 to program it. I removed all J101 jumpers and connected GND, 3V3, RST, TMS, TCK, TDO, TDI pins to my board.
With a new MSP432 on the board, I can connect and program code, but only once. When I try again, I get "CS_DAP_0: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 9.2.0.00002)".
I have tried to reset to factory settings: when I right-click on the XDS110 CS_DAP_0 in the Non Debuggable Devices section, and attempt to Connect Target, I get the Error -261 and can't run the reset script.
Test Connection works.
I have changed the JTAG/SWD/cJTAG option to every option except cJTAG 2 pin mode, and have set a few fixed JTAG TCLK frequencies (various, from 100 kHz to 5.5 MHz), and still get a successful connection test and no connection on the CS_DAP_0 in the Non Debuggable Devices.
CCS 10.0.0.00010
MSP432P4111IPZ, LFX 32.768 kHz, HFX 24 MHz, LDO only