Hi Team,
Good day! Need your expertise on our customer's inquiry below:
"I have a question about ADC capturing of TIDM-1019. My system's TOF is about 7us and I wanna capture echoes using internal ADC but there is a parameter in GUI called "Gap between pulse start and ADC capture(us)" with minimum value of 20 (in Water Mode), so I think ,I will loss the first reflected wave!
Now the first question is this, What's the minimum TOF that MCU can calculate and also how can I capture input waveform using internal ADC when the TOF is 7us?
Could I capture 14'th echo (reflected wave) ,If I set the parameters like this:
Transmit frequency = 1MHz (T = 1us and TOF = 7us, so the first reflected wave will received at 7us and 14'th reflect at 20us)
Gap between pulse start and ADC capture(us) = 20
Number of Pulses = 30 and more ?
Is there any better solution?"
Kind Regards,
Jejomar