Other Parts Discussed in Thread: MSP430FR2522, MSP430FR2633, MSP430FR2533, MSP430FR2532, MSP430FR2632,
I was reading through the captivate headers and found this in CAPT_ComConfig.h
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I was reading through the captivate headers and found this in CAPT_ComConfig.h
Hi John,
I believe that is an oversight. The MSP430FR2512 configuration needs to be added in the CAPT_ComConfig.h.
Yes, it's unfortunate for this small pin count device that the default BSL pins happen to share a Captivate pin.
My suggestion would be to modify the CAPT_ComConfig.h to meet your needs.
According the MSP430FR2512 datasheet, BSL is supported using the following pins:
Hi John,
P2.4 is fine. Be sure to configure this as your interrupt pin in the CAPT_commConfig.h and check that this pin is configured as an "INPUT" in the BSP.h. This sets the pin up as a psuedo open drain configuration. When its time to generate the IRQ the I2C driver will re-configure this pin as an output,drive the pin low, wait for a time out then re-configure back as input.
**Attention** This is a public forum