This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 55
Part Number: CC1200
Hi, My customer is using CC1200 with 1800pF as an external loop filter capacitor. (the capacitor connected between pin23:LPF0 and pin24:LPF1) Suppose the capacitor value is different, what parameters are impacted and how? For example, if 470pF or 10nF are used mistakenly. Thanks and regards, Koichiro Tashiro
Typically this will be seen on the output spectrum. The output signal will not have the correct shape if this component has a wrong value.