Part Number: MSP432P401R
Tool/software: Code Composer Studio
HI,
Today I was testing how EnergyTrace works with my devices: MSP432P401R + CC2650MA + Educational MKII and I have some questions:
- I have observed that using a simple program as Blink, if I disconnect the Educational MKII, there are -30mA of consumption. Is there any way of have it plugged but programatically disabled or try to reduce its consumption if it is not being used as this case?
- After use some times EnergyTrace, I think that my CC2650MA is not working. I have tested BLE examples and no one is working. The program is waiting forever at this instruction: "Semaphore_pend(waitRsp_sem, BIOS_WAIT_FOREVER);". Could you confirm to me that I need a new one module or could be problem of the MSP432P401R?
- If I remove all the modules and test the blink with EnergyTrace, now it looks as if not enough power is provided. This is one graphic:
In addition: this is a video observing the same issue but with the educational mkii plugged:
However, if I don't use EnergyTrace, any program (not related to BLE) is working ok. I have installed and uninstalled the CSS 2 times and the same is happening. So, I don't know if Bluetooth module is broken or the MCU or both. Could you help me?