Part Number: MSP-EXP432P401R
I have an MSP-EXP432P401R Rev 1.0 board (the dark gray one, before they started being made on a red board).
I am unable to connect to it with my Mac laptop - no USB port is created. I have a MSP-EXP432P401R Rev 2.1 board (red colored) that has no issue connecting with the same cable plugged into the same USB port, but swap the boards and it doesn't work.
All jumpers are "jumped" between the XDS110-ET side of the board and the MCU side.
I get a green and red LEDs blinking on the MCU side of the board (the blinking may be may last uploaded program) - the point being that the MCU side of the board is receiving power
BUT the XDS110-ET side of the board has not LEDs lit up - I think a green one is supposed to light up and I get that on the other, Rev 2.1 board.
So it is clear that power is getting to the board as a whole, and the cable works, but the Rev 1.0 board does not seem to be presenting as a USB port, so I don't know how I could refresh firmware or do anything else.
The TI website says that the MSP-EXP432P401R is not supposed to require any drivers on a mac - and the Rev 2.1 connects fine.
Help is appreciated :-)