Hi
Is the following external oscillator available?
- which include Spread spectrum function
Center Spread: ±0.25%, ±0.5%, ±1.0%,±1.5%, ±2.0%, ±2.5%
- Freq: 24MHz
Thanks and Best regards,
HaTa.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Is the following external oscillator available?
- which include Spread spectrum function
Center Spread: ±0.25%, ±0.5%, ±1.0%,±1.5%, ±2.0%, ±2.5%
- Freq: 24MHz
Thanks and Best regards,
HaTa.
Hello Hata,
I'm not sure I understand your question. Are you asking for an external HF crystal recommendation or something about the FR5738 crystal support?
Thanks
JD
Hi JD
My question is if FR5738 can work with the external crystal which contains the following features.
- which include Spread spectrum function
Center Spread: ±0.25%, ±0.5%, ±1.0%,±1.5%, ±2.0%, ±2.5%
- Freq: 24MHz
Our customer has the exact crystal product in their mind, and they would like to know if it's available with FR5738 or not.
Thanks and Best regards,
HaTa.
I’ve looked at this oscillator spec, and we don’t specify anything about center frequency spread, but we do specify max frequencies. Table 5.14 shows max frequency of 24 MHz input. Also, it’s noted that the “max frequency of operation the entire device can not be exceeded.” This is give in the Recommended operating conditions as 24MHz.
Therefore, they shouldn’t use any crystal that has a chance of being over 24MHz. I think they should lower the center frequency of their crystal to leave room for these crystal tolerances. As for the spread of the crystals, that shouldn’t have any impact on the MSP430 as an MCU, but they may notice these timing differences in their application since the MSP430s will be running at varying speeds. If their application can handle the +-2.5% variation in frequency, then it should be fine.
Thanks,
JD
Hi JD
Do you agree that, for example, we set the down spread from 24MHz to -1.0%, and use software to handle it?
**Attention** This is a public forum