Other Parts Discussed in Thread: EVM430-FR6043
Hello.
I would like to achieve same or less than 10ms measurement period.
In GUI, UPS0 to UPS1 gap is set to 20ms, but the gap of UPS0 pulses and UPS1 pulses is 38ms.
Then I confirmed below, and I understand wakeup and processing overhead takes about 18ms.
Is my understanding correct?
Software version is UltrasonicGasFR6043_02_30_00_01
Are there any solution to achieve 10ms measurement period?
For example, I don't need average TOFF and average Flow Rate.
Looking at the source code, it seems that the average process using 100 pieces of data is repeated many times in order to calculate the Average TOF and Average Flow Rate.
Is it possible to achieve a measurement cycle of 10 ms or less by omitting these processes?
Regards,
U-SK