Hi.
I have some questions regarding the calculation of the absToF. Is the maxLobe mentioned in https://www.ti.com/lit/an/slaa889/slaa889.pdf?ts=1610816769623&ref_url=https%253A%252F%252Fwww.google.com%252F calculated for every peak in the ADC capture or just till the max. value for the peak is reached?
I'm wondering because i did some measurements under zero flow conditions and measure the signal in parallel with a oscilloscope with 8 GSa/s and the ToF calculated by the EVM is smaller compared the ToF measured with the Oscilloscope. I set the threshold for the Oscilloscop to 0.1 and the 'Envelope Crossing Threshold' parameter is set to 10. That means 10% of the max, right?
The difference between both ToF's is in the range of 1 µs. In the USS all offset parameters are set to 0. Target of this test was to determine the delays and offset times for my setup.
Maik