Hello support team.
I am using the MSP430FR2355 VQFN-32 and I want to confirm if it is possible to connect Timer0_B3 and Timer1_B3 in cascade without the need to connect external pins.
Looking at pages 73 and 74 of the datasheet, it looks like Timer0_B3's CCR2 can take the Timer1_B3_INCLK output.
I intend to configure Timer0 to be the LSB, receiving SMCLK of 25 MHz and Timer1 receiving the overflow of Timer0 and being the MSL of a 32 bit counter.
Could you confirm me if this is possible without connecting external pins and don't want to take advantage, could you tell me the values of the Timer0_B and Timer1_B registers that I should configure?
Best Regards.