Hi,
We are planning on using the CC430F6137 Reference Voltage (pins 59/60) as a reference for a DAC7513 digital to analog converter. Specifically, we're planning on connecting pin 59 (VREF+) on the CC430 to pin 3 (VREF) on the DAC7513. Could you please answer the following questions when you get a chance?
1) We were planning on having the CC430 and DAC7513 share the same ground. Is it alright if we connect pin 60 (VREF-) on the CC430 to this shared ground plane? Or, should we have a seperate analog ground for VREF- and the DAC7513?
2) What capacitance is recommended between VREF+ and VREF-? We were thinking of putting a 470nF capacitor between these pins (59/60) near the CC430 and then putting a 100nF capacitor between VREF and ground near the DAC7513. Does this sound reasonable?
3) How much current can the CC430 VREF+ pin supply?
Thanks for your time.
John