In an application I need to send data to a PC wirelessly.The main unit consist of MSP-FET430U80 target board featuring MSP430FG439 micro controller.I thought of sending the data first to ez430-RF2500 target board via wired interface,then that EZ430 target board will communicate with EZ430-Rf2500 USB stick module with another EZ430 target board attached to the same USB stick so that data can be send to the PC.
Will this set up work OR I need to modify somewhere?