From the user guide, I have noticed the register to be 8 bit.
My doubts are :
- Does setting each bit represent the interrupt action in the corresponding pin of the port ?
- If so, can only one bit be SET in the PxIFG register at a time ?
- Till a bit which was SET in PxIFG is cleared, won't interrupts in other pins in the same PORT be handled ?
- Will the state of P1IFG affect configuring P2IFG ?