Other Parts Discussed in Thread: TIDA-00120, SM72295
Tool/software: Code Composer Studio
Dear sirs,
I build a project PMP7605 with GUI according to TIDA-00120 Solar MPPT Charge Controller Reference Design ... the code was loaded to target (MSP430F5132), the charge controller work not properly ....when debug I take many errors...it seems to me some problem with compiler...the most errors are: ....variable xx , is used as a constant. recommend declaring variable as either 'static' or 'const'....another error...detected SW delay loop using empty loop. recommend using a timer module instead....also one of three warnings .....this project was created using a version of compiler that is not currently installed -4.1.5 (MSP430). another version of the compiler will be used during build - 18.12.2.LTS....from CCS installation details already installed MPS430 compiler tools v. 18.12.2... (is different with 18.12.2.LTS ?). its about compiler , or something else ? if so, what is the suitable compiler and how can I update ?
another question is : can I use the solar controller board without TIDA-00120 GUI connected after edit some parameters? can I start the charge with edit of code ? is it possible to control the charge without GUI ?