This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5132: Do I have an option of reprogramming microcontroller pin to UART module?

Part Number: MSP430F5132

Greetings ,

For a project I am using MSP430F5132IDA microcontroller. The design is taken from TI. I am attaching schematic of micro-controller section with this post.schematic-4.pdf

My issue is that I am very new to this micro-controller(have previously used only TM4C from TI) and also my project deadline is 1 week only. I have to implement UART communication on this controller with available pins. So can I connect UART module to available pins using port mapping controller?

Thanks

Best Regards

Bhushan