This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2617: MSP430F2617TPM and MSP430F2617TZQW - Reading hardware revision information using the CPU

Part Number: MSP430F2617
Other Parts Discussed in Thread: MSP430FR6922

Hello,

I have a question regarding accessing hardware revision information from the MSP430F2617 devices.

I need to detect via uC software that the application is running on either the MSP430F2617TPM (64-PIN LQFP) or the MSP430F2617TZQW (113-PIN BGA)

Therefore if the uC software detects the BGA device then we can use PORTS 7 and 8.

Some of the MSP430 devices contain Hardware revision information stored in the Tag-Length Value (TLV) structures. For example the MSP430FR6922 contains Hardware revision and Die Record information.

Is there someway (other than using an external pull-up/pull-down resistor) to detect the MSP430F2617TPM and MSP430F2617TZQW devices using uC software ?

Is there Hardware revision information available to the CPU for both of these devices ?

Hoping you can assist me with this matter.

Kind Regards

Brendan

**Attention** This is a public forum