Hi,
we use the integrated temperature sensor with the calibration data from TLV. Unfortunately the results are not as expected.
cal30 (1.5Vref) @ 0x1A1A 2114
cal105(1.5Vref) @ 0x1A1C 2683
We followed the sample code and got the following measurement results:
Temperature [degC] | Measured ADC data | Calculated temp [degC] |
30 | 2115 | 30 |
105 | 2614 | 95,5 |
As you can see, ADC measurement result at room temperature (30 degC) is accurate and nearly matches the calibration data 2114 from TLV.
When measuring at 105 degC, the measurement result does not match the calibration data 2683 from TLV.
Why the measured value differs so much?
Is there someting wrong with the reference point at 105 degC or just inaccuracy of the sensor at high temperatures ?
We expected more accurate temperature data when using two point calibration, particularly at the two calibration points.
Regards,
Ralph