Other Parts Discussed in Thread: DRV8711,
Tool/software: Code Composer Studio
Hi all,
I am having MSP430G2 Launchpad and DRV8711 boost pack to run the stepper motor.
I am using CCS10.0.0.00010
I downloaded the reference files (application and GUI) from the website
https://www.ti.com/tool/BOOST-DRV8711
As mentioned in the DRV8711 user guide, I used method 2 for importing the ccs project and downloaded to MSP430 Launchpad. This is fine no issue noticed during application loading.
Now I want to open the GUI composer, where it is?
In CCS, view->GUI composer->Designer (Online) is only available. In that if I select the "import existing project and select BOOST-DRV8711_GUIv1.0.exe" it shows as
"FAILED TO EXTRACT PROJECT FILES. REASON: ERROR: INVALID SIGNATURE 0x905a4d"
Can anyone suggest how to run the stepper motor in following two conditions:
1) MSP430 Launchpad + DRV8711 boos pack with GUI (ie GUI for setting the parameters and start stop command)
2) MSP430 Launchpad + DRV8711 boos pack without GUI (ie In MSP code itself for setting the parameters and GPIO to start/STOP)
Thanks and Regards,
Iyyappan.V
Iyyappan_krish@yahoo.co.in