Other Parts Discussed in Thread: MSP430F2617, MSP-FET
Tool/software: Code Composer Studio
Cannot program the MSP430F2617 on the development board with code-composer studio, CCS.
Power was applied to the VBAT terminal and the supplied mini USB cable was connected to the development computer.
When trying to program/debug CCS was unable to connect to the device.
I did NOT installed the GUI that can be used to interface and control the motor driver. (Do not need it.)
OS: Windows 10.
CCS: Version: 10.0.0.00010
Is there a driver that needs to be installed for CCS to be able to program/debug on the MSP430F2617 installed on the development PCB? Or, does kit DO NOT support debugging with CCS?