This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: External loop filter component

Part Number: CC1200

Hi,

My customer is using CC1200 with 1800pF as an external loop filter capacitor.
(the capacitor connected between pin23:LPF0 and pin24:LPF1)

Suppose the capacitor value is different, what parameters are impacted and how?
For example, if 470pF or 10nF are used mistakenly.

Thanks and regards,
Koichiro Tashiro

**Attention** This is a public forum