Hello,
I'm in the process of trying to flash a microcontroller in Code Composer Studio 6. When I'm debugging the code, I get the following message:
Error initializing emulator:
A firmware update is required for the MSP430 Debug Interface (MSP-FET430UIF / MSP-FET / eZ-FET). Click the "Update" button to update the firmware and launch your debug session (this may require several update steps).
DO NOT UNPLUG THE INTERFACE DURING THE UPDATE.
Afterwards, I go to update it, only for the firmware update to stop, with the next error message appearing:
MSP430: Error: MSP-FET430UIF Firmware erased - Bootloader active
This happens every time I select the debugger in an attempt to flash the program onto the microcontroller. I don't know what the issue is, or how to solve it, so I'm looking for any advice that could help me solve this problem.