Hello,
What is the quiescent current of the integrated 3.3-V LDO inside the MSP430F5326?
What is the current when no load?
Why is it ON at power on?
Best regards
Mich
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What is the quiescent current of the integrated 3.3-V LDO inside the MSP430F5326?
What is the current when no load?
Why is it ON at power on?
Best regards
Mich
Hi MichRFT,
There isn't a spec in the datasheet, which tells me it is not tested/measured in production so not sure. I'll have to reach out to our product team in Asia to see if that information is available.
I believe it is enabled by default for a scenario where 5v is the system power and the LDO output powers the MSP430. You want the LDO on by default so the MSP will power up. If you are providing a separate 3.3v from another source, then the LDO should be disabled.
Hi MichRFT,
It's been a few days since I have heard from you so I’m assuming your question has been answered.
If this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information.
If this thread locks, please click the "Ask a related question" button and in the new thread describe the current status of your issue and any additional details you may have to assist us in helping to solve your issues.
Hi MichRFT,
Sorry it has taken a while to get this information.
Ok, the spec is 60uA. The F5326 is a non-USB derivative with the same internal 3.3v LDO as shown here.
If you have the power system configured as shown in the NON-USB illustration and measuring the input current on the LDOin pin, then if the CPU is in a LPM3 mode (CPU, MCLK, SMCLK off) you should measure around 60uA. What exactly do you measure?
Can you provide details on your power system and how you are measuring your currents. What is the application?
**Attention** This is a public forum