Other Parts Discussed in Thread: TIDM-1019
I have two questions about the application note.
1.Liquid Level Sensing
https://www.ti.com/lit/an/slaa951a/slaa951a.pdf
From the application note 2 Test result, it is stated that it can detect 50 ns absolute time, while Figure 2-2 only detects 5us time.
Do you have any information if 50ns detection is feasible?
2.Oxygen Concentration Sensing
https://www.ti.com/lit/an/slaa976/slaa976.pdf
In the application note 1 Introduction, there is a description of "measurement periods of less than 10 ms".
Does this statement mean "UPS to UPS1 GAP =10 ms"?
If so, please tell me the specific setup procedure.
Thanks,
Koki