Hello
I have problem with MSP430G2402IPW20
I using the Iar system in assembler only and just using may item of msp430 family, model F, G and Fr too from long time.
now I using MSP430G2402IPW20 and have probelm with emulation, I using it at 12 mHz with internal calibrtation ,
and running properly and I use also the information memory like eeprom memory..
The problem is that if I leave the watchdog disable I can put many brekpoint without any problem
and all running properly, but if I enable watchdog and put any breakpoint immediately have a reset,
If do not put any breakpoint running properly , this is a problem for emulation.
for Emulation I using Iar embedded workbanch 6.50.1
may be I make mistake can yuo help to understand were ?
thank you
Luigi