Hello,
I would like to use BSL UART and SPI.
BSL UART is used for programming firmware at mass production.
So in PW16 package, 11 pin and 12 pin are used.
SPI is used for application to communicate other MCU.
So I am considering following pin assign.
1pin : SCLK
15pin :SIMO
16pin :SOMI
Is this use case no problem?
Regards,
U-SK