This thread provides a list of all FAQs related to MSP-EXP430G2 LaunchPad. If you find any useful bits of 'hidden' information whether from your experience working with the part, or from a question or an issue that was resolved, please reply to the thread. Remember this is not a place to ask questions for specific issues, but to gather information that LaunchPad developers might find helpful. This first post serves as the master list and will be updated every so often to include new found FAQs.
Requently Asked Questions (FAQ)
1. Does the MSP-EXP430G2 support fuse blow?
The MSP-EXP430G2 LaunchPad experimenter board onboard debugging interface lacks the JTAG security fuse-blow capability. To ensure firmware security on devices going to production, the USB Flash Emulation Tool or the Gang Production Programmer, which support the fuse-blow feature, are recommended.
2. Can other programming tools like the MSP-FET430UIF interface the MSP-EXP430G2 LaunchPad socket device?
The LaunchPad experimenter board works with any programming tool supporting the 2-wire Spy-Bi-Wire interface. Both the MSP430 USB FET (MSP-FET430UIF) and the Gang Programmer (MSP-GANG430) support these devices, but the connection must be made directly to the dedicated Spy-Bi-Wire ports. See MSP-FET430 Flash Emulation Tool User's Guide (SLAU138) for details on using MSP430 USB FET and the Gang Programmer for a 2-wire Spy-Bi-Wire interface. Don't try to connect the standard JTAG connector to the MSP-EXP430G2 pinheads, as this could result in damage to the attached hardware.
3. What versions of IAR Embedded Workbench and Code Composer Studio are supported?
The MSP-EXP430 LaunchPad hardware is supported by IAR Embedded Workbench KickStart Version 6.00 and Code Composer Studio v4 or higher. To download the software and for more information on the supported software visit the LaunchPad Wiki page.
4. What are the part numbers for the connectors between the LaunchPad emulator board and the other eZ430 target boards?
Header: Mill-Max 850-10-006-20-001000
Socket: Mill-Max 851-93-006-20-001000
5. I am not able to select the MSP430 Application UART and cannot receive data.
Ensure that the Application UART driver is correctly installed. This is done by installing either IAR Embedded Workbench or Code Composer Studio v4.
To determine if the driver is correctly installed:
a. Plug in the MSP-EXP430G2 LaunchPad with the included Mini USB cable.
b. Right click My Computer and select Properties.
c. Select the Hardware tab and click on Device Manager.
d. Under Ports (COM & LPT) should be an entry for "MSP430 Application UART (COM xx)".
If the entry is there, but no characters are received, reconnect the LaunchPad to the PC and restart the application to reload the drivers. If the Application UART is not listed, install the driver by following the instructions in Section 2.2 of the User's Guide.
6. The device is not answering to any communication, JTAG or UART.
If you are experiencing difficulties in communicating to the attached MSP430 target device, even though all the communication drivers for the MSP-EXP430G2 are loaded correctly, the emulator is probably set to a wrong communication state. This can be fixed by reconnecting the LaunchPad Experimenter Board and restarting the communicating application.