This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: Clarification on analog input clamp current

Part Number: TMS570LS1224

Hi Team,

Our customer would like to confirm about the analog input clamp current stated in the datasheet and errata.

I am using TMS570LS1224 and in the datasheet the information about "Analog input clamp current" is, that it is some value when input voltage exceeds Vccad + 0,3V. In Errata there is some additional information about injecting current into an input channel and it says that it happens when the input voltage exceeds Vccad - 0,3V....

I would like to make sure that the info in Errata is correct and it is really Vccad - 0,3 V and not Vccad + 0,3V. Could you advise on that?

Thank you for your support!

Regards,

Danilo