Are there any plans to make a BOOSTXL-IOBKOUT - GPIO Breakout BoosterPack without the Voltage Follower Op Amps? In my opinion making the BOOSTXL-IOBKOUT - GPIO Breakout BoosterPack with the Voltage Follower Op Amps was a poor decision. I just spent the weekend unsoldering the Op Amps and adding jumpers on 3 of the boards so I could use the BOOSTXL-IOBKOUTs with a BOOSTXL-SENSHUB and other applications that need those pins for non-analog I/O. The Op Amps could have been easily added externally if required. Also why only one VBUS pin and so many 3.3V?